Other Parts Discussed in Thread: TPS7A30
Hello im a beginner at designing electronic circuits and the following questions might have an obvious answer i did not see.
While designing a low noise filter for an op amp i think i came across an inconsistency in your data sheet for the TPS7A49 and im not sure how to proceed now with my design. In the datasheet on page 14 under adjustable configuration equation 2 writes: V(FB nom)/R2 > 5 μA
But when looking at the Userguide on page 3 the R2 changes to (R1 + R2) for the TPS7A49. Also for the TPS7A30 datasheet the equation is with (R1+R2).
Which one is it?
Another thing that confuses me in the data sheet for the TPS7A49 is on page 17 equation 5 where this is used to calculate the resistors. For R1 we calculate it to 1.265 kΩ but in the next sentence R1 is now set at 68.1 kΩ?
kind regards
Nicolas