Other Parts Discussed in Thread: TPS92200, TPS54200
Hello:
Two low-voltage circuits(using LM3414MRX/NOPB) need parallel output. Can they be used in this way? Thank you!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Sorry for replying late...
Could you help explain why two LM3414 need to be connected in parallel? Is larger output current wanted?
Robin
Hello Yuting
The power supply current of the lamp board needs 1.5A, and the maximum output of LM3414 is only 1a, so I want to use two channels of output 750ma in parallel to supply the lamp board,Is it feasible?
Hi Jimmy,
I think it should work but I haven't tried this before, so I can't guarantee it. How about TPS92200 or TPS54200/1?
Robin