Part Number: BQ24650
I am using this part as in the attached schematic to charge a lead acid battery from a solar panel.
I want to set a maximum charge current of 10 amps as per the datasheet section 8.3.3. where Icharge = 40mV / Rsr
When testing the design, I find that I am only getting about half of my expected charge current and that the voltage across R122 is a bit under 20mV where I expect it to be around 40 mV.
I am using 1 110W solar panel or 2 of these in parallel.
I selected the resistor divider on MPPSET to give me about 1.2v as per the datasheet with my input voltage at appx. 18v and my MPPSET pin is around 1.2v during operation.
I suspect that the part may be regulating / reducing my charge current as per section 8.3.2 of the datasheet but I don't see why as my solar panels should be able to produce the required energy in full sunlight.
I would also like to clarify how to calculate Vrech. I want to set my Vrech threshold to 14.8v and my Vlowv threshold to 8v if that is possible.
All help appreciated, thanks in advance