This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS274160: Timing issues

Part Number: TPS274160

Hello,

At the TPS274160 datasheet, it is stated that the Td,rise,  is maximum 150uSec. 

But dV/dton, which is one of Td,rise parts, is 0.1V/uSec, which means that with 24V supply, the rise time from 10% to 90% can be 240uSec.

In this case the Td,rise should be maximum 90uSec + 240uSec = 330uSec, which is larger than the stated 150uSec.

Am I missing something?

Thanks,

Asaf