This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713B: Need latest Linux driver of battery charger chip BQ25713BRSNT

Part Number: BQ25713B
Other Parts Discussed in Thread: BQ25710, BQ25713, EV2400

Hi , 

I am using  Battery charger BQ25713BRSNT from Texas instruments  for Table PC application .  

Battery pack  is made with  2 series  Li -PO batteries (2S1P ( 2series)  of   max. voltage of 8.4V ,capacity 3400mAh.

We need latest  Linux driver of BQ25713BRSNT for integration with host CPU . Please help at the earliest . 

Regards

Sudheer George

Innominds Software  Pvt Ltd.

www.innominds.com

  • Hi,

    Thanks for reaching out.

    We don't provide any reference drivers for this part, please refer to register map section of the datasheet. However, a third party open source reference may be available such as:
    https://chromium.googlesource.com/chromiumos/platform/ec/+/master/driver/charger 

    The BQ25710 is similar to BQ25713 but BQ25710 is SMBus based. Please note that TI does not guarantee the functionalities of the third party reference.

    We have a dedicated GUI for users to quickly evaluate our evaluation modules and learn our chargers. Noted that the EV2400 interface does not come along with the EVM and must be purchased separately.

    Thanks and I hope this helps,

    Peng

    *Please press "This Resolved My Issue" on the thread if my answer is satisfactory