Other Parts Discussed in Thread: TPS54560, TPS54560B
Dear team
The customer would like to know, what is the difference between TPS54560 and TPS54561?
Could you help to recommend?
Many thanks
Denny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Denny,
The TPS54560 is not recommended for new designs. I'd suggest look at the TPS54560B instead and this is p2p compatible with TPS54560.
The TPS54561 is a 10 pin device which has a controllable softstart pin, while the TPS54560/B is a 8 pin device without controllable softstart.
If customer cares about inrush current or providing power supply sequencing, then I'd suggest using the TPS54561 10 pin device.
Regards,
Jimmy