Hi team,
Our customer design an Inverting power supply with LMR23625C.
When the load current is over about 100mA, the current consumption is over 1A.
We share the schematic in the follow figure. Could you check the schematic and comment concerned this issue?
design condition
Vin: 15V @ Regulated power supply
Vout: -10V
Iout: 700mA
note: When this issue occurred, we observed the Vout is -10V. And When there is no load, the device package become hot about 50-60℃.
If the Thermal PAD is not connected to PGND and AGND enough, is it possible the current flow the PAD or other root?

Best regards,
teritama