This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2546-Q1: Does it detect SDP/CDP/DCP when device is connected @ auto DCP?

Part Number: TPS2546-Q1

Hi team,

Does it detect SDP/CDP/DCP when device is connected @ DCP auto?
In addition, how do I configure CTL pin to detect SDP/CDP/DCP detection if DCP auto mode do not have this feature?

I thought "this device at first detect which SDP/CDP/DCP is required, if it detects DCP, then it operates as suitable DCP mode such as divider1, divider2, and so on.
However, D+ and D- voltage looks 2.7V/2.0V instead of 0.6V...

Regards,
Ochi