Other Parts Discussed in Thread: BQ40Z50, , EV2400
For 2s, 3s and 4s battery configurations, how does the BQ25798 manage charge balancing such that each cell's voltage is balanced?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
That's what I thought, when I saw nothing about that in the bq25798 datasheet. I'm looking to charge and balance two 18650 Li-Ion batteries in a 2S configuration. What separate IC do you recommend that would go with the bq25798? I would like to get something that could do 3S or 4S as well, for other projects. Please let me know. Thanks, Carl
Hi Carl,
There is no reference design with the 798. It is too new. I have forwarded to a coworker who is more familiar with the gauge and balancing ICs. Hopefully he can direct us to a reference design with another charger and possibly a better option for balancing IC.
Regards,
Jeff
Hello Carl,
There's no specific reference design that uses them both together, essentially what you would do it connect PACK- on the gauge to the PGND on the charger and PACK+ to BAT. I attached a very simple block diagram for the connections.
After the battery is fully learned (SLUA903) you can set the balancing to be enabled and the gauge will perform passive cell balancing as described in section 7.1 of the TRM https://www.ti.com/lit/pdf/sluua43
The TRM is the best source of information for cell balancing using the gauge.
Sincerely,
Wyatt Keller
Wyatt, I don't see where the bq25798EVM has SMBC and SMBD connections. I do see the I2C connections for SCL and SDA. Is that what should be connected to the bq40z50EVM's SMBC and SMBD connections, respectively?
Carl
Hello Carl,
Yes the BQ25798 uses I2C, the diagram I shared is for a similar setup, all the connections should be the same besides the names. SCL = SMBC, SDA = SMBD is correct.
Sincerely,
Wyatt Keller