Other Parts Discussed in Thread: TIDA-010208
Hello
I have two questions; the first I think is obvious or a misinterpretation by me of the datasheet. The second question requires some knowledge from the designers to explain if my requirement is feasible.
Q1.
From bq76952.pdf, Page 74, "Table 16-3. Terminating Unused Pins"
"
Recommendation:
Cell inputs 1, 2, and 16 should always be connected to actual cells, with cells connected between VC1 and VC0,
VC2 and VC1, and VC16 and VC15. VC0 should be connected through a resistor and capacitor on the pcb to
pin 17 (VSS).
"
I want to use a single connector with increasing connector size for 3S, 4S, etc and install it at the correct location on the "full" sense connector pads on the copper.
I intend to use a common copper layout and configure the board for 3S to 16S by installing zero ohm resistors in the filter capacitor locations to connect VC sense pins to adjacent pins. Unused sense resistors are not fitted.
For a 3S pack, I am unsure what the recommendation means; is it ok to connect pack terminal 2P to the VC2 sense pin and use the zero ohm links to connect all VC pins VC2 through to, and including, VC15 ? Is there any sensing and/or balancing current requirements for a "direct" connection of 2P to VC15 rather than to VC2 when they are linked together ?
I will still have the filter capacitors VC1 to VSS, VC2 to VSS, and VC16 to VC15 and sensing/balance resistors between VC0, VC1, VC2, and VC16 to their respective pack terminals.
Q2.
Can I improve top and bottom cell voltage measurement by making VC0 and VC16 a sense wire out to the battery terminal (cutting netlinks on the copper) rather than connect to BAT- and BAT+ on the PCB using the Netlinks on the copper ? I respect that voltage drops across the pack power cables will impose negative voltages on VC0 referenced to VSS but that is the point of removing voltage drops over the high current cables to the top and bottom cells. Is the requirement to connect VC0 on the copper because damage or bad measurements are possible with VC0 and VC16 as sense wires ?
Apologies if these questions have been address in another forum post. I looked at most BQ76952 questions and didn't see them.
All the best
Harry