Hi,
I want to enable a soft start to the EVM output voltage and not a hard start directly to 12V. The user guide is this:
How can I do this while using an external MCU (MSP432 Launchpad) and J2 header on the EVM. Can I use the SS pin on J2 header in any way?
Also, how can I use the TRIm pin on the J2 header to det the otput votlage from an external MCU (MSP432 Launchpad)?