Other Parts Discussed in Thread: BQSTUDIO, , EV2400, BQ40Z50
Hi,
I'm developing a 2s3p pack using the BQ40z50-R1. I'm using a BQ40z50EVM to preliminary tests. In my first test I was trying to connect the EVM with the BQStudio using a EV2400 and 2 cells in series, but the Bqstudio accuses that was no device connected. I was only able to communicate with the EVM using 4cells in series. After that, I changed the DA config to work with 2 cells and now everything is working properly.
I wonder if I need to leave connections on my PCB project to connect a 4s pack during the first BQ40z50 communication with the BQStudio or if I had bad luck with this EVM and the ICs in general can communicate with the BQStudio using a 2s pack since the first connection.
Thanks.