I have a bq20z75 that will not enter sleep mode. The SMBus lines are tied to ground with 1M resistors, the SMBus master clock and data lines are set low, and there is less than 10mA current flow (650uA). The SLEEP bit is set in Operation Cfg A and NR is set in Operation Cfg B. There are no PF or Safety Status flags set.