Hi, support team
My customer has the questions as follow:
Here are some problems on my short circuit boardand.
Problem:
When I use an energy harvester to connect Vin (Vin is about 5V),
the capacitor on Vbat cannot be charged;
when I use a battery for charging,
it can work normally.The capacitance on Vbat is 2200uF,
and the output uses 10K ohm resistive load
Could you help to solve?
Thanks so much.
Best regards,
Yuki