This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25069: Recommended external MOSFET for 16.5A Iout application.

Part Number: LM25069
Other Parts Discussed in Thread: TPS25982, CSD17570Q5B, CSD16415Q5

Hi team

Could you help check if LM25069 + CSD17570 is suitable for 16.5A Iout application?

  • Vin=12V&5V
  • Iout=16.5A

The customer prefers to hot-swap device with internal MOSFET, but we only have 15A max. TPS25982 now.

Considering the presence of margin for output current spec, it seems that solution using external MOSFET would be more reasonable.
Hence I am wondering if you could help check if LM25069 + CSD17570 is suitable for this requirement? These devices are already used in my customer.

 

Let me know if you have any questions.