This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Boost IC for LiDAR] Boost Converter recommendation inquiry

Hi, TI Support Team

Customers are looking for products that satisfy the following conditions.

Please recommend a product that satisfies the application and specifications.

[spec]

- Input Voltage. : 5V or 12V

- Output Voltage : 42V or Higher(48V)

- Output Current : 3A or more

[Application]

- LiDAR for vehicle / LiDAR for serving robot

Thanks.

Regards,

MJ