Hello,
We are planning on using the DCP020515DP in our motor controller design, and we have some questions.
The datasheet states that the isolation voltage between input and output is minimum 1kV RMS (1s Flash test, 60s test UL1950).
· What is the continuous isolation voltage rating?
The continuous differential the device will be seeing in our application is 300V continuous between input and output. How do we know that the device can handle it?
- The operating temperature range is -40 to 85°C. Can you provide derating curves for usage above 85°C ?
Regards,
Albert WOROU