Other Parts Discussed in Thread: INA226
I have a problem using MPSoC with TPS6508641 and I ask questions.
There are two products that operate normally, and for bad board, the current consumption appears abnormally high.
For debugging, I removed the power sequence output sequentially.
Initially, after removing the output of the BUCK1, I measured the consumption current to verify the difference between the normal and bad board, both of which were the same.
Next, after removing the output of BUCK2, I measured the consumption current, and the results were similarly the same.
And then, after removing the output of the BUCK5, I measured the consumption current and the current of the bad board was confirmed to have risen rapidly.
The problem here is, I don't know if the MPSoC's power block using 0.85V as the power source is the problem or PMIC's BUCK2 0.85V output is the problem.
(0.85V is not used other than MPSoC supply power.)
I would appreciate your help.
Thank you.