This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563210A: what is high side FET VDS rating

Part Number: TPS563210A


Hi team,

May I know what is high side FET VDS rating of TPS563210A? (VIN-VSW)

My customer is testing VDS for both high side and low side FET, we have VSW rating 19V max(DC) and 21V max(10ns transient), but I can not find high side FET VDS spec.

Thank you.

Regards,

Allen

  • Hi,

    I think you can directly use the Absolute Maximum Ratings spec of the input pin, which mean Vin Max=Vds highside max=Vds low side max=19V. This is the max stress that will be put on the high side FET(Acutally, between the low side FET turn on and the high side FET turn off, the stress will be Vin+Vdiode low side,which is a little bit higher ), it will happen during the on period of the low side FET.

    I'm not sure about what do you want to test.

    Thanks!

  •   Allen,

    Since the VIN to SW rating is not listed separately, it's a safe assumption that theirAbsmax ratings will be similar, 19V DC 21V for <10ns transient.

    Keep in mind, the Absolute Maximum rating is not the same as a Vds breakdown rating.  The Absmax rating will always be lower than the breakdown voltage, though the amount of margin can vary from design to design and with normal processing variations.  The actual breakdown voltage will all be above the 19V rating with typical break-down voltages a few volts higher. 

    A word of caution testing the exact Vds break-down - keep the source current for testing the break-down small, recommended less than 100μA with as little external capacitance as possible while testing.  There are additional circuits attached to the VIN net that could avalanche before the primary power FETs during a slowly rizing VIN above 21V, and the FETs can experience "Snap-Back" after exceeding their break-down voltage.  During Snap-back, the avalanche voltage of the MOSFET decreases, which can discharge external capacitance and a large external capacitor could deliver excessive energy to the FET devices, damaging them.

    During a fast rising VIN (<10ns) such as an ESD event, the primary MOSFETs or the ESD protection devices will trigger first first, and hold the VIN voltage below the threshold of these other, lower current paths until the ESD energy is dissipated, but during a slowly rising DC threshold test, process variations can result in those other paths triggering first.

  • Hi Peter,

    My customer is measuring ringing spike of high side, what is the test criteria we should follow? 19V or 21V.

    Thank you.

    Regards,

    Allen

  •  

    They should be following both.

    If the voltage ever exceeds 19V, it should not exceed 19V for more than 10ns, and it should never exceed 21V.