Other Parts Discussed in Thread: TMCS1101
Hello.
Please tell me about the Advanced Current Synthesizer Current Sensing, which is a feature of the UCC28070A.
I know the benefits of using a current transformer.
In UCC28070A, the drain current of MOSFET is detected by the current transformer,
and the current flowing through the boost diode is produced by the synthesizer.
Even if you don't bother to use synthesizer functions,
I think that the necessary information can be obtained by changing the position of the current transformer,
inserting the current transformer in series with the inductor,
and detecting the current.
Why do you need this feature?
What are the advantages and disadvantages of using this function?
When RSYNTH is connected to VREF, connect CSA and CSB directly to their respective current amplifiers.
When do you use this function?
For example,
TMCS1101 1.5% Precision, Basic Isolation Hall-Effect Current Sensor
Is it a case of using?
I think that using TMCS1101 is easier to design and smaller than preparing a current transformer,
but please give me some advice if you have any precautions.
Thanking you in advance.