Part Number: TPS55288
Hi E2E,
What are the factors needed to consider in selecting the MOSFET for TPS55288? Is the on-resistance below 7mOhm acceptable? What is the Gate-Source voltage?
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Carlo,
When selecting the MOSFET for TPS55288, you have to consider below specs:
1. The MOSFET Vgth max is better less than 3V. Because the TPS55288 driver voltage is 5V.
2. It's trade of selecting the on-resistance. The MOSFET conduction loss is related to on-resistance, which MOSFET reverse recovery loss is related to Qrr.
3. As TPS55288 VCC capability is 60mA, two external MOSFET driver current = 2*Qg*fsw. Make sure driver current is less than 60mA.