This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV103: DRV103

Part Number: DRV103


Hello.

 I am using the DRV103 for the one of my application for the break enable and disable.

In DRV103 Pin 1 connected to 91K ohm resistor for 30%duty cycle.

                   Pin 2 connected to 100nF/25V Ceramic capacitor  for 100ms Dealy.

                   Pin 3 connected to 205K resistor for frequency setting.

                  P-ch MOSFET part number is  IRF9Z24N

I am getting the delay  100ns Correctly but, after the delay PWM  voltage is +15 V to -16V coming.

Can any one  suggest why these is happen.