Other Parts Discussed in Thread: LM61460, LMR36520
Hi expert
I have a requirement raised by our customer that they are conducting a wireless charger project and want you to recommend a proper DC-DC for them, here are the features they need:
• constant voltage output (adjustable 3-40V): the maximum output power can be 50W;
• Output voltage adjustment method: IC with communication port is better, and it is also OK without it;
• Priority recommendation of H-Bridge driver type and Automotive level device needed;
Thank you!