Hi team,
The following are some questions about the use of LDOs for BQ76952 to power MCU, could you please give some comments?
Thank you.
1. When the BQ76952 is powered on for the first time, what are the default states of the two LDOs and the output voltage values?
2. When BQ76952 is initialized, what are the default states of the two LDOs and the output voltage values?
3.When the BQ76952 freezes, what is the default state of the two LDOs and the output voltage value?
When the freezes resumes, what is the default state of two LDOs and the output voltage value?
The above problem stems from the impact of the BQ76952 on the MCU, which may leave the MCU power off in an uncontrolled state.
Regards,
Ivy