This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61391: TPS61391: current monitor connected to transimpedance converter

Part Number: TPS61391

Hi together,

at the moment we are busy designing an APD power supply with output voltage trimming depending on sereveral environmental conditions. Voltage adjustment works as expected using and external DAC. But we struggle using the current monitor outputs.

Instead of using resistors connected to GND to convert current into a voltage we want to use a transimpedance converter as shown in the picture below:

OPamp ist single supply powered with 3.3V. Reference voltage on the p-Input is 1.0V.

Are there any restrictions when conneting to a amplifier like that? Do we have to keep anything in mind that is not part of the TPSxx's datasheet like limits for current sourcing or sinking or anythng else?

We are looking forwad to your answers?

Thanks for your help and yout hints in advance.

Best

Christian