Other Parts Discussed in Thread: TPS27081A
Hi Sir,
We are trying to use TPS27082L as an alternative source for the TPS27081A.
In the characteristic and peripheral circuit of components portion, does there any concerns we need to pay attention to?
TPS27082L internal block diagram as following table's right side.
Shall we change R109 to 0R ohm? Because it has internal PD 12.5K ohm already?
And as a Spec. recommendation change R108>150K ohm?
Or we can install TPS27082L on the location U15 directly and keep the peripheral circuit setting?

Regards,
Joseph Liao