Hi All,
I am using the bq20z45R1 in a 2-cell application with LFP cells. When I power up the device, I am not able to change from the default 3-cell configuration in Operation CFG A to the 2-cell I need (Operation Cfg A = 0x0129) because of flags due to cell undervoltage and over temp on TS2. I only want to use TS1 in my aplication. When I go through the bqEasy steps, I am also not able to write to dataflash because of the CUV flags being set. Instead I get a DFF PF flag. Is there an overwrite to ignore the flags in order to configure the dataflash?
TL