This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180: 120VAC input, 300V DC output, 1800W

Part Number: UCC28180


Hi,

       My customer is using UCC28180 for a new design: 120VAC input ,300V DC output, 1800W, PWM 5Khz.  please kindly suggest if UCC28180 is suitable one. 

BTW, they met two design questions:

1.the external components of ICOMP and VCOMP is diffcult to caluate, do you have suggestion how to easy to get these values?

2.according to datasheet,VCOMP is 3V, but in M1 calulation  , the value used is 2.45V, they want to know how this 2.45V come from?