This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMPS Design 230VAC to 24VDC with 4A current



Hi,

I want design SMPS as per below details, pls suggest any ICs.

Input Voltage: 150V to 300VAC

Output Voltage: 24VDC

Output Current: 4A

Secondary side regulation

Low space design

Anyone help.