Hi there , I attached the problem in the below document .Is there a way test each section individually and find the cause of this behavior?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there , I attached the problem in the below document .Is there a way test each section individually and find the cause of this behavior?
Hi Pradeep Would you please check these items on-by-one ?
Eric Lee (Applications Engineer)
Hi Eric, Thanks for your timely reply.
Hi Pradeep
EP should be connected to ground. The device temperature will be higher than expected if the EP is not connected to a large ground plain. It also can cause a malfunction when switching noise exists.
Eric Lee (Applications Engineer)
Hi Pradeep
Because I haven't heard about any VCC pin failure which is caused the device itself until now and the device has been in production since 2007, I think the issue might be caused by an error (either by a wrong component selection or a wrong connection on PCB).
Please check these items.
Thanks
- Eric Lee (Applications Engineering)
Hello Pradeep
Since both VCC and VCCX are not connected to VOUT, I think there is no possibility that the loop instability causes the VCC pin damage. Just to make sure, I suggest you to populated the unit (whose VCC is 9V) on other working board and double check if the VCC voltage is still 9V or not.
Thanks
- Eric Lee (Applications Engineering)
Hi, I'm afraid we ran out of all IC which we had used during testing but our order is in transit. We will make this test once we get our components with us. Moreover we are designing new board only for the buck converter. Once the design is done, Can I share the file with you so that you can review and suggest some changes if something exits?
Thanks
Hello Pradeep
Sure, please open new thread with the file when it is available. I can review them.
If you don't want to post the file in public forum, please contact your local FAE and send the file to the FAE, then we can discuss via email.
I am closing this thread.
Thanks
- Eric Lee (Applications Engineering)
Hello Pradeep
No, the reverse recovery current of D5 doesn't cause SW overshoot or VCC capacitor over charge. If an excessive reverse leakage current of D5 can overcharge the VCC capacitor.
Thanks,
-Eric Lee (Application Engineer)