Hi Team,
Customer wants to check our internal LDO VCC voltage and min Toff time, which is not mentioned in Datasheet, could you help to provide these data? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I will check with the internal system and design time to see if there are any called out spec for this device.
As you've mentioned the datasheet doesn't provide any clear parameters/specs for what you are looking for.
When I get more information on this I'll get back to you.
Regards,
Jimmy
Hi,
I just sent another reminder to the team.
Again thank you for your patience and sorry I couldn't get to this database and get you the information sooner.
These specs are not listed in the datasheet so only the designers can some idea of what these specs are.
Regards,
Jimmy
Hi,
Regards,
Jimmy
Hi Jimmy,
Thanks for your update. I also want to check the BOOT charge output voltage for TPS54561. Because in 7.3.4, I can't understand this equation well, does it mean VBOOT-SW or VBOOT-GND? if it means VBOOT-SW, when Vin>11V, VBOOT-SW>8V, over spec; if it means VBOOT-GND, when Vin=20V, Vboot=14.76V< 20V Vin.
Thanks for your help.