This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63030: Maximum soft start delay

Part Number: TPS63030

Is it possible to mention the maximum soft start delay from VEN high to VOUT valid?

For example, it does not exceed 1 msec.

<Conditions>

VIN: 3.0-5.5V

Operating temperature: -45-85 degree C

VOUT residual voltage: 0-4.0V

The measurement data is attached below.

/cfs-file/__key/communityserver-discussions-components-files/196/Soft-start-delay-on-TPS63030EVM_2D00_417.pdf

(R1 and R2 is adjusted so as to be 4.0V in the attached data.)