Dear Expert,
Good day!
I have 2 questions about the TPS51220A here ,
1 . from the datasheet reference design, it said the Vo1 and Vo2 support max output current is 8A , But form the calculation on the datasheet ,the Iocl(peak)=VOCL * 1/ Rs *( Rx + Rc)/ Rc
base on the parameter on the schematic , Vocl = 60mV ,Rs = 10.5 mR ,Rx = 7.5k ,Rc = 4.3K, So I peak= 15.68A ,even though IOCL(PEAK) should be approximately 1.5 × IOUT(MAX) to 1.7 × IOUT(MAX). the result is Iout (max) is 15.68/1.5(1.7) = 9.2-10.45A , it is not same to the datasheet descriptions , could you tell me is there any mistake I had made ?
2.What is the difference between non-droop in Current Mode and standard Current Mode?
BR,
Leon.liu