Other Parts Discussed in Thread: TPS61175
Hi TI team,
The unit of Sn and Se is not the same. I think the equation for Sn is correct because I saw it here https://www.ti.com/lit/an/slva452/slva452.pdf?ts=1631189220487&ref_url=https%253A%252F%252Fwww.google.com%252F.
But I am not 100% sure of Se. What is the unit Se? Is there a missing unit in the equation? More importantly I want to confirm if the equation is correct.

Secondly, in the TPS61178 datasheet, it says:
Note that if Sn > Se, e.g., when L is too small, the converter operates as a voltage mode converter and the above model no longer holds.
But I saw the opposite statement on TPS61175 datasheet. Yes, they are different controller but I think the working of the current-mode slope compensation theory to be the same, so I kind of expect the statement should be the same too. Appreciate if you can confirm if the statement in TPS61178 datasheet is correct.
And if the statement is correct, it doesn't say anything about what model to use if it behaves like voltage-mode controller. I am completely lost there. 
Lastly, if TI has a calculator spreadsheet to calculate the compensation values, I would like to get my hands on it. Thank you.