Part Number: BQ40Z50-R3-DEVICE-FW
Hi
I have two questions about the sustained peak power (SPP) and maximum peak power (MPP) values for Turbo mode feature.
1. What are the conditions that SPP and MPP would report 0? Here are the conditions that I can think of: Update status is not 0x0E, SBS.RSOC = 0%, reaching the terminate voltage, Vload is lower than Min System Voltage. Are there any other conditions would cause SPP and MPP become 0?
2. What would be the conditions that SPP and MPP values will be the same?
Thanks.