I have a small PCB designed and assembled to evaluate the TPS61040 for a client. The input is from a Lithium Titanate battery (2.4V) and the output is set to 3.3 Volts to power the MCU.
Please ignore the input/output voltages on the above clip of the schematic, the specification changed since the drawing was done.
For testing the battery is replaced by a bench PSU, set to 2.4 volts. With no load connected I an seeing the correct voltage (3.3 volts) however, on my scope I see a sawtooth wave for of around 30Hz and 600mV peak to peak.
Also, I have noted that with a load of 100mA the output voltage falls well below 3.3 Volts.
Any help you can provide would be much appreciated.
Sid