This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: clear interrupt after power up

Part Number: TPS6594-Q1
Other Parts Discussed in Thread: TDA4VM

Hello team,

Customer use TPS65941212+TPS6594111 to power TDA4VM, system could power up successfully but they see some interrupt after power up:

TPS65941212     

0x5A:0x18; 0x65:0x02; 0x66:0x01

TPS65941111     

0x5A:0x14; 0x63:0x08; 0x64:0x02; 0x66: 0x01

GPIO2 connect to SD_VOLTAGE_CTL

Two questions regarding to the interrupt:

1. How to clear 0x65 fault of 1212? Customer write 1 to clear fault but it will shut down the PMIC immediately, according to d.s, the ENABLE_INT should be status indication only which will not impact the state machine.

2. For all those interrupt, should customer do it manually after power up or it's integrated in the latest SOC driver?

Thanks.

Dongbao