IN THE DATASHEET, COMPONENT VALUES ARE GIVEN UP TILL 9V BUT SPEC SAYS IT CAN WORK UP TO 16V OUTPUT
ALTHOUGH I CAN CALCULATE IT,
I WOULD LIKE TO KNOW WHY 12V OUTPUT WHICH IS A VERY COMMON OUTPUT VOLTAGE IS NOT INCLUDED
ARE THERE SOME CONSTRAINTS?
MY DESIGN HAS A 15V 2A INPUT AND I NEED A 12V 1A OUTPUT WITH A 6.8UH INDUCTOR THAT CAN OPERATE UP TO 1MHZ AND 1x 0.1uF CERAMIC + 2x 22uF MULTILAYER SMT CAPS
PLEASE ALSO GIVE ME THE VALUE FOR Cff OR CAN IT BE OPTIONAL LIKE THE FIXED VOLTAGE VERSION.
WHY IS THERE NO SIMULATOR OPTION FOR THIS PART?
THANKS
JOHN