This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61220: Did TPS61220 support 1.2V output

Part Number: TPS61220
Other Parts Discussed in Thread: TPSM82822, TPS82085, TPS61094, TPSM82823, TLV627432

Hi Sir,

In our new project, there is a requirement for DC to DC. The input voltage is required to be 0.9V~2.7V, and the output voltage need to be 1.2V or 1.5V fixed output, but if the feedback resistance is adjustable (we tend to adjust it to 1.2V) ).

We learned that the minimum output voltage of the TPS61220 is 1.8V, but the feedback voltage is 0.5V. And we want to use the 1Mohm and 1.4Mohm resistors to divide the voltage to achieve a 1.2V output. Can u help to confirm whether this is feasible? The calculated value is OK, but does not meet the minimum output of the chip.

Thanks,

Kind Regards

  • Hi Lumina,

    Thanks for reaching to us. Please based on electrical characteristics to use this device. With low output voltage there might be some internal block mal-functioned. Boost converter is not like to buck converter, which typically as minimum Vout as same as reference voltage. As some of internal block is supplied by Vout and Vin is only used for start-up, so Vout has typically higher minimum Vout than reference.

    What is your output load requirement? TPS61011 may be a good choice, but i need to know if you have more specific requirement like device package, output current.

    -Wenhao

  • Hi Wenhao,

    The end equipment is cap pencil and the load current is no more than 300mA. We fristly thinking about the buck converter, but found no buck products with 1.2V output on TI's official website. Can u give us some better suggestion?

    Thanks,

    Best Regards

  • Hi Lumina,

    I think may be you have improper search setting. There are a lot of buck devices supporting down to even 0.6V output, like TPS82085, TPSM82822/3, etc, but which needs higher input voltage than 0.9V to 2.7V so you may need a boost converter to boost up bus voltage for down streaming loads. This is the first thing that strikes me.

    However, considering you are design cap pencil which may need lower solution size. (I would appreciate you can share some image link of the product or similar, just curious. ) I need to check if there is any single stage solution which could support your application so that you can save your size at maximum.

    I will feedback to you before tomorrow. Thanks!

    -Wenhao

  • Hi Wenhao,

    Our cap pencil is similar with Apple pencil and the width of PCBA is about 4*4mm, so there are certain requirements for the package size of DC to DC.

    I have checked the datasheet of TPS82085 and TPSM82822/3 on TI website, but the height is not suitable.

    Thanks,

    Kind Regards

  • Hi Lumina,

    What is the input power of the cap pencil? Supercapacitor? Or battery or from an adapter?

    -Wenhao

  • Hi Wenhao,

    The input power of the cap pencil is supercapacitor, and the voltage range from 0.9V to 2.7V.

    Thanks,

    Kind Regards

  • Hi Lumina,

    Got it. I checked internally and there is no Boost or Buck-boost converter available at such a low voltage operation. I would recommend TPS61094+Buck converter/module or LDO.

    Do you have specific requirement on height? Since you have said TPSM82823 does not meet your requirement. I can help check if any Buck converter can meet your requirements.

    -Wenhao

  • Hi Lumina,

    Per we talked, I would recommend customer a boost converter solution + a buck converter solution

    TPS610992+TLV627432 remains the smallest and the lowest input solution which can help you in their device. We will try to touch with your customer for further information. Thanks!

    -Wenhao

  • Hi Wenhao,

    Thanks a lot. I will pass on your suggestion to our customer.

    Best Regards