Other Parts Discussed in Thread: UCD9090
Hello we are using an I2C master (PCA9564) to communicate to the UCD9090A. It is a parallel to I2C bus controller.
Can we use standard I2C commands to communicate with the UCD9090A or do we need to use PMBus commands.
We are simply doing a read of the I2C bus (using address 104d) and we are not seeing an ACK from the UCD9090A.
We are sending a start/slave address/read and we do not get an ACK back.
Do we need to setup the UCD9090A in a way to ACK this command?
I have already programmed the UCD9090A Fimware with the Interface adapter and the firmware controls my PDN rails. we are now adding in a way to communicate with the UCD9090A in system without using the interface adapter.
Regards,
Guy