We are using UCD9248PFC for sequential control of power. However, there were often cases where normal power was not output from the voltage converter, which caused problems with the reliability of the system. It was confirmed that the PWM signal was not normally output and was set as a low signal if the cause was not operated while identifying the cause. However, in some cases, it may operate when rebooted again. I want to hear your opinion on this.