This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563249: Alternate of TPS563249 due to unavailabilty.

Part Number: TPS563249
Other Parts Discussed in Thread: TPS563201, TPS56339

Hi,

My customer is using TPS563249 for generating a 5V output rail from a 12V input. The maximum output current required is 2A. But the Supply of TPS563249DDCR is highly constrained. Can you suggest some alternatives to the customer?

Thanks & Regards,

Jash 

FAE