Other Parts Discussed in Thread: , BQEVSW, BQSTUDIO
Hi,
Customer is want to confirm what datasheet they need to used. Below is the details.
"
I am currently interfacing with the BQ34Z100 over I2C. Upon reading the DEVICE_TYPE control function, I get returned `0x100`, implying that the device is a BQ34Z100-G1. However, when I read flash subclass 48, I see that the string `bq34z100` is at offset 46 in the subclass 48, implying that I am talking to a BQ34Z100 device as according to an outdated version of the datasheet. Therefore, I have no idea which datasheet I should refer to for the correct register information, as the most recent datasheets say that I should expect to see the string `BQ34Z100-G1` at offset 31 in flash subclass 48, but that is not the case. For reference, I bought the device from this DigiKey purchase link: https://www.digikey.com/en/products/detail/texas-instruments/BQ34Z100PWR/3305538.
"
I have found that there is error in the datasheet and the correct device type for this device is 100 based from this link 5 years ago:
Can I recommend to the customer to use the outdated version of the datasheet?
Regards,
Maynard