Part Number: LM5085-Q1
Other Parts Discussed in Thread: LM5085
Hi,
We are trying to use LM5085 DC-DC buck driver as buck constant current driver for LEDs. We are using Op-Amp and sense resistor to sense output current, Op-Amp output voltage is connected to Feedback pin. Also please note that the output current through LED is around 850mA. We have used voltage divider to limit maximum output voltage in case of LED Open circuit. In case of LED load connected the output voltage is up to 11.5V and In case of open load(led not connected) output voltage is 16V to 17V(Set by using Voltage divider and Diode D2). For more details please go through attached circuit diagram.
Is there any problem if we use LM5085 as constant current driver?