This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320: GPI signal does not shutdown a rail.

Part Number: UCD90320

Hi,

I have a temperature fault signal defined on several GPI pins (in my design TEMP_ALERT_FP0-4 on GPI 11-15). If this signal goes high, a rail must shutdown.

See definition below.

Then in the Rail configuration->fault responses tab:

Here I set the GPI11-15 to shutdown the rail. The problem is that when a GPI pin goes high, nothing happens? But the rail shut shutdown....

What am I doing wrong?

Preview attachment UCD90320 @ PMBus Address 113d Project.xml

UCD90320 @ PMBus Address 113d Project.xml
882 KB

Kind regards,

Ben