Hi,
After finishing the learning process, I extracted the golden file but forgot to set the LStatus bit to 2 (turn off IT Gauging). Can this result in Full charge capacity not being correct when programming the golden file into another BQ Chip? On the new chip, the fcc is displayed as 5331mAh instead of ~11900mAh as was on the EVM board after the learning process was finished. Sending the RESET command does not change this.
Another golden file was read from the same EVM board with the LStatus bit set to 2, but the battery was disconnected and then reconnected to the board. So I don't know if this golden file is valid for use.