This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090: What is the default status of UCD9090 Alert pin?

Part Number: UCD9090

Hi there,

the UCD9090 alert pin was pull-up to 3.3V by a 10Kohm resistor.

what is the defaut status of the alert output? Is it high or low without loading any configuraiton?

My UCD9090 alert output keeps low while I download the configuration.

Best Regards,

York

  • Hi

    Alert is a open drain signal. if it is low, it means something happen.

    If there is no configuration, the ALERT is low to indicate that it is a blank device. 

    But once the configuration is programmed and reboot, the ALERT shall be HIGH.

    Regards

    Yihe