This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92630-Q1: Review of the LED lighting issue schematic.

Part Number: TPS92630-Q1

Hi,

Customers have a problem that LEDs are not turned on during product production.

The LED is not turned on like the video on the link.

KakaoTalk_20210910_143601558.mp4 18MB

Test method.

1. All LEDs on through four ICs after 2 seconds of power application.

2. When you touch the touchpad switch, LED dimming is performed in the order of 70% -> 40% -> OFF -> 100%.

3. The dimming PWM frequency is 490 Hz.

4. TPS92630 of the four, a specific IC does not turn on.

5. Positions where each board is not turned on are different.

There are cases where it is turned on when the power is reset.

It is not turned on during the repeated test.

The FAULT status is Low, and I don't know the cause of FAULT.

Please guide us on the improvements to solve the symptoms.