This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MOSFET alternatives

Hi 

I received a BOM from a customer and I would like to ask if you could suggest some alternatives.

These are the parts:

  • SI9435DY 
    MOSFET 30V 5.1A 2.5W P-channel
  • bss138  
    MOSFET, n-channel, 50 V, 220 mA, 3.5 ohm, SOT-23, 
  • BSH105215
    MOSFET N Channel Mosfet SOT 23

Thanks and Regards

Alex