Hello:
My client uses BQ25892 in POS Project.
The abnormal charging mode is detected. When the battery power reaches 96%, the charging will be intermittent. What is the reason?
The customer feedback that there is no abnormality in hardware measurement . It is inferred that it is a software problem
The customer thinks this problem may be related to the triggering of ICO mode at 95%. There are several points my client wants to confirm:
1、what is the detailed working mode of ICO mode?
2、Why set 95%?
3、Whether this phenomenon is a normal behavior in ICO mode
4、What will happen if ICO mode is turned off?
Thank you